Hello all, Im trying to run qemu for emulate a "hello world" for T2080.
I succesfully installed all the SDK and run host-prepare.sh script that say me everything is OK.
$ source ./fsl-setup-poky -m t2080rdb
$ bitbake fsl-image-virt
Im trying to run:
$ ~/SDK/QorIQ-SDK-V1.7-20141218-yocto/poky/build_t2080rdb_release/tmp/sysroots/i686-linux/usr/bin/qemu-system-ppc64 - cpu e6500
And the output is :
"Unable to find PowerPC CPU definition"
I also try differentes qemu builds with no luck, for example: ~/SDK/QorIQ-SDK-V1.7-20141218-yocto/poky/build_t2080rdb_release/tmp/work/i686-linux/qemu-native/1.7.0-r0/qemu-1.7.0/ppc64-softmmu
I also check that meta/conf/bitbake.conf has the next lines:
QEMU_OPTIONS_e6500 = "-cpu e6500"
QEMU_OPTIONS_e6500-64b = "-cpu e6500"
If i try to boot qemu without -cpu option, qemu just freeze without any text output:
(qemu) QEMU waiting for connection on: telnet:0.0.0.0:4444,server
Warning: vlan 0 is not connected to host network
Here is the script where i try to run on qemu:
#!/bin/bash
rd=~/SDK/Target_Images/PPCE6500_Images/t2080rdb/fsl-image-core-t2080rdb.ext2.gz
kernelimg=~/SDK/Target_Images/PPCE6500_Images/t2080rdb/uImage--3.12-r0-t2080rdb-20141213024927.bin
sudo ~/SDK/QorIQ-SDK-V1.7-20141218-yocto/poky/build_t2080rdb_release/tmp/sysroots/i686-linux/usr/bin/qemu-system-ppc64 -nographic -m 256 -M ppce500 -kernel $kernelimg -initrd $rd -append "root=/dev/ram rw console=ttyS0,115200" -serial tcp::4444,server,telnet -net nic
I Tried differents kernel configurations, even using qemu-system-ppc instead of 64 bits version, and i don't have any output.
Best Regards,
Daniel.