Hi,
Sorry I write a terrible english.
I work in the project using XMC CPU module (XPedite6101 from X-ES) containing a T1042 processor.
We use the SerDes configuration 0x88. With the XMC module there are two RGMII link with BCM5482S PHY, two SGMII phy-less, and one SGMII with marvell 88e1111.
I have a problem with the SGMII to Marvell 88e1111. The CPU doesn't not manage the MDIO, this is a Kintex FPGA which drives the MDIO line.
I configured the PHY in SGMII mode, 1000Mbits, with auto-negotiation.
I tried some DTS configuration but it doesn't work.
Firstly, I want to know if my DTS is configured correctly.
Currently the DTS looks like this:
enet0: ethernet@e0000 { | |||
cell-index = <0>; | |||
compatible = "fsl,fman-memac"; | |||
reg = <0xe0000 0x1000>; | |||
fsl,port-handles = <&fman0_rx0 &fman0_tx0>; | |||
fixed-link = <1 1 1000 0 0>; | |||
phy-connection-type = "sgmii"; | |||
ptimer-handle = <&ptp_timer0>; | |||
}; |
enet1: ethernet@e2000 { | |||
cell-index = <1>; | |||
compatible = "fsl,fman-memac"; | |||
reg = <0xe2000 0x1000>; | |||
fsl,port-handles = <&fman0_rx1 &fman0_tx1>; | |||
fixed-link = <2 1 1000 0 0>; | |||
phy-connection-type = "sgmii"; | |||
ptimer-handle = <&ptp_timer0>; | |||
}; |
enet2: ethernet@e4000 { | |||
cell-index = <2>; | |||
compatible = "fsl,fman-memac"; | |||
reg = <0xe4000 0x1000>; | |||
fsl,port-handles = <&fman0_rx2 &fman0_tx2>; | |||
fixed-link = <3 1 1000 0 0>; | |||
phy-connection-type = "sgmii"; | |||
ptimer-handle = <&ptp_timer0>; | |||
}; |
enet3: ethernet@e6000 { | |||
cell-index = <3>; | |||
compatible = "fsl,fman-memac"; | |||
reg = <0xe6000 0x1000>; | |||
fsl,port-handles = <&fman0_rx3 &fman0_tx3>; | |||
phy-handle = <&phy0>; | |||
phy-connection-type = "rgmii"; | |||
ptimer-handle = <&ptp_timer0>; | |||
}; |
enet4: ethernet@e8000 { | |||
cell-index = <4>; | |||
compatible = "fsl,fman-memac"; | |||
reg = <0xe8000 0x1000>; | |||
fsl,port-handles = <&fman0_rx4 &fman0_tx4>; | |||
phy-handle = <&phy1>; | |||
phy-connection-type = "rgmii"; | |||
ptimer-handle = <&ptp_timer0>; | |||
}; |
mdio@fc000 { | |||
#address-cells = <1>; | |||
#size-cells = <0>; | |||
compatible = "fsl,fman-memac-mdio"; | |||
reg = <0xfc000 0x1000>; | |||
interrupts = <100 1 0 0>; |
phy0: ethernet-phy@1 { | ||||
reg = <0x1>; | ||||
flags = <0x2>; | ||||
}; | ||||
phy1: ethernet-phy@2 { | ||||
reg = <0x2>; | ||||
flags = <0x2>; | ||||
}; | ||||
}; | ||||