T2080E SVR value unexpected/doesn't match the docs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080E SVR value unexpected/doesn't match the docs

833件の閲覧回数
ascii
Contributor I

Hello,

Per the reference manual (rev 1) the SVR for the T2080E should be 0x853800xx, however I have a customer with a core that is reporting 0x85780011. Is there any explanation as to the difference, especially with regards to JTAG/COP connections? They're having problems connecting to their board via JTAG and this appears to be the only thing out of place. Thanks.

Regards.

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)