T2080 board ethernet port 2 ping failed 2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 board ethernet port 2 ping failed 2

1,618 次查看
jiachaozhang
Contributor II

The board is T2080RDB

now, we erase the u-boot,both current and alternate. Please give me the related recovery image files to recovery u-boot.ufedor

标签 (1)
标记 (1)
0 项奖励
回复
9 回复数

1,197 次查看
ufedor
NXP Employee
NXP Employee

Complete T2080RDB NOR Flash image (QorIQ_SDK_V2.0_T2080RDB_20160527_NOR_Flash.bin) is included into the "QorIQ Linux SDK v2.0 PPCE6500 IMAGE" ISO which could be downloaded from:

https://nxp.flexnetoperations.com/control/frse/download?element=7726177 

0 项奖励
回复

1,197 次查看
jiachaozhang
Contributor II

You have been redirected to this page because your ID is INACTIVE in Flexera. Please Activate your account to proceed.

If you believe you have reached this page in error, please contact NXP® Technical Support.

 

what's this?

0 项奖励
回复

1,197 次查看
ufedor
NXP Employee
NXP Employee

This means that you have to register.

0 项奖励
回复

1,197 次查看
jiachaozhang
Contributor II

Hello! I register a new account.

recovery the u-boot use usb tap with code warrior.But today i erase the RCW. The usb tap can not connect the board,the message is"Failed to reset the target"

I need program RCW without u-boot,where can i find T2080RDB_RCW_override.cfg,and please give me detail operation description.

0 项奖励
回复

1,197 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the attached screenshot.

0 项奖励
回复

1,197 次查看
jiachaozhang
Contributor II

debug ok,but cann't write rcw!     

write_rcw.JPG

0 项奖励
回复

1,197 次查看
ufedor
NXP Employee
NXP Employee

1) Please confirm that "_Connect" Debug Configuration was modified for the RCW override.

2) After establishing Debug Connection (using the RCW override "_Connect" configuration) ensure that the board initialization script was executed properly and SDRAM memory is operational.

0 项奖励
回复

1,197 次查看
jiachaozhang
Contributor II

what is the board initialization script?

How to make SDRAM memory is operational?

0 项奖励
回复

1,197 次查看
ufedor
NXP Employee
NXP Employee

The board initialization script is defined here:

2018-05-08_191319.jpg

> How to make SDRAM memory is operational?

Please try to perform memory writes and check the results.

0 项奖励
回复