The board is T2080RDB
now, we erase the u-boot,both current and alternate. Please give me the related recovery image files to recovery u-boot.ufedor
Complete T2080RDB NOR Flash image (QorIQ_SDK_V2.0_T2080RDB_20160527_NOR_Flash.bin) is included into the "QorIQ Linux SDK v2.0 PPCE6500 IMAGE" ISO which could be downloaded from:
https://nxp.flexnetoperations.com/control/frse/download?element=7726177
You have been redirected to this page because your ID is INACTIVE in Flexera. Please Activate your account to proceed.
If you believe you have reached this page in error, please contact NXP® Technical Support.
This means that you have to register.
Hello! I register a new account.
i recovery the u-boot use usb tap with code warrior.But today i erase the RCW. The usb tap can not connect the board,the message is"Failed to reset the target"
I need program RCW without u-boot,where can i find T2080RDB_RCW_override.cfg,and please give me detail operation description.
debug ok,but cann't write rcw!
1) Please confirm that "_Connect" Debug Configuration was modified for the RCW override.
2) After establishing Debug Connection (using the RCW override "_Connect" configuration) ensure that the board initialization script was executed properly and SDRAM memory is operational.
what is the board initialization script?
How to make SDRAM memory is operational?
The board initialization script is defined here:
> How to make SDRAM memory is operational?
Please try to perform memory writes and check the results.