[T2080] : Unable to connect CodeWarrior JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[T2080] : Unable to connect CodeWarrior JTAG

433件の閲覧回数
Arathi
Contributor II

Hi NXP Support Team,

I am using NXP T2080 processor card and CodeWarrior TAP JTAG to connect to the processor.

I have created a new bareboard project for QorIQ target following new project wizards from File->New->CodeWarrior Bareboard Project Wizard.

When trying to connect CodeWarrior to the target from Run->Debug Configurations->CodeWarrior-><project>-core0_SRAM_<processor>_Download->Debug, Unable to connect

Please find the below Error observation:

  1. While connecting via CTAP [UART] :
     Error launching t2_demo-core00_SRAM_T2080_Download
    CCSProtocolPlugin : Could not connect to the probe (or other debug link)
    [CCS last error: CC driver failure ]
  2. While connecting via Ethernet :   
     Error launching t2_demo-core00_SRAM_T2080_Download
    CCSProtocolPlugin : Resource unavailable
    [CCS last error: Resource Unavailable]

On the CCS console tried giving the below commands still the result was resource unavailable

delete all
config cc cwtap
ccs::config_chain t2080
ccs::reset_to_debug
source IDcode.tcl

Please do help us resolve this issue

Thanks and Regards,
Arathi

 

 

 

 

0 件の賞賛
返信
1 返信

340件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that there is problem with CCS USB driver on your host.

Please reinstall CodeWarrior for PA 10.5.1 on other host.

And change for other CodeWarrior TAP to do verification, it seems there is problem with your CodeWarrior TAP itself.

0 件の賞賛
返信