T1040 voltage ID feature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1040 voltage ID feature

跳至解决方案
1,385 次查看
fdm
Contributor IV

Hi,

There's no mention of the voltage ID feature in the current revisions (rev.1) of the T1040 Data Sheet and Design Checklist.

But the T1040 Reference Manual says that "Boot software must read FUSESR and translate the values into the appropriate commands to set the voltage output value of an external voltage regulator."

Is that requirement of the voltage ID feature usage really mandatory for the T1040?

Regards,

Denis

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,222 次查看
ufedor
NXP Employee
NXP Employee

The voltage ID has been defeatured for the T1040.

The cited RM statement has to be discarded.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,223 次查看
ufedor
NXP Employee
NXP Employee

The voltage ID has been defeatured for the T1040.

The cited RM statement has to be discarded.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------