Board: T4240RDB
SDK: QorIQ-SDK-V2.0-20160527-yocto
The default version for Linux kernel is 4.1.8. I want compile a new Linux kernel with version 4.1.3. How can I modify the files inside the SDK? I have tried some recipes under 'sources/poky/meta/recipes-kernel/linux/'. However, it doesn't work. Is there any suggestions or where can I find some documentations?
解決済! 解決策の投稿を見る。
Hello Junjie Shi,
Please refer the following method.
Please clean the Cache
$ bitbake virtual/kernel -c cleansstate
Get the source of Kernel
$ bitbake virtual/kernel -c patch
Please go to Linux Kernel source folder build_t4240rdb/tmp/work/t4240rdb-fsl-linux/linux-qoriq/4.1-r0, please remove git folder, then copy and rename your Kernel source folder as git.
If you want to configure and rebuild Linux Kernel, you could use this method.
$ bitbake virtual/kernel -c configure
Please go to the folder build_t4240rdb/tmp/work/t4240rdb-fsl-linux/linux-qoriq/4.1-r0/build
$ make ARCH=powerpc menuconfig
Got to build_t4240rdb
$ bitbake virtual/kernel
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
yipingwang Thanks a lot for your answer! However, I still have a problem when doing the menuconfig: if I come to the folder build_t4240rdb/tmp/work/t4240rdb-fsl-linux/linux-qoriq/4.1-r0/build and do '$ make ARCH=powerpc menuconfig', there is the menuconfig for kernel 4.1.8 rather than the kernel 4.1.3 in folder 'git'. If I come the the git folder, and do 'make menuconfig' directly, then there is the correct menuconfig window. The configure for the kernel is important for my project, how can I correct this problem? Thanks in advance for you help!
Hello Junjie Shi,
Please refer the following method.
Please clean the Cache
$ bitbake virtual/kernel -c cleansstate
Get the source of Kernel
$ bitbake virtual/kernel -c patch
Please go to Linux Kernel source folder build_t4240rdb/tmp/work/t4240rdb-fsl-linux/linux-qoriq/4.1-r0, please remove git folder, then copy and rename your Kernel source folder as git.
If you want to configure and rebuild Linux Kernel, you could use this method.
$ bitbake virtual/kernel -c configure
Please go to the folder build_t4240rdb/tmp/work/t4240rdb-fsl-linux/linux-qoriq/4.1-r0/build
$ make ARCH=powerpc menuconfig
Got to build_t4240rdb
$ bitbake virtual/kernel
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------