Does the T1024 have the Aurora interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the T1024 have the Aurora interface?

Jump to solution
673 Views
Larry5335
Contributor IV

The block diagrams, Ref Man and data sheet all show it. Does Aurora really exist on the T1 series parts?

Labels (1)
Tags (1)
0 Kudos
1 Solution
514 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024 has the Aurora interface as it is shown in the manual. The Aurora port on the T1024QDS is implemented using the T1024 Aurora interface.
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
515 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024 has the Aurora interface as it is shown in the manual. The Aurora port on the T1024QDS is implemented using the T1024 Aurora interface.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos