hi,my version of CodeWarrior Development Studio For PA is 10.4.0 and I use the evaluation version.However, I encountered an error as shown below:
If you can help me answer this question, I would be very grateful.
Hi,
You're using CW for PA v10.4.
The evaluation version includes a 30 days professional license file.
When the evaluation time expires the tool will work at Special Edition level with is free of charge but limited.
According to the license file it seems the evaluation time expired the January 1st 2015.
Since the 2nd January the tool is working at special edition level.
I don't remember what was included in Special Edition for PA V10.4 and the info is not anymore available on web (contacted the team to solve it).
For me, the error message you met is normal as the evaluation time expired.
Now the question is: did you purchased a suite ?
CW for PA V10.5 is the last version.
This version is available under CodeWarrior Development Suite for Networked Applications.
For details I recommend you to refer to the web link:
CodeWarrior Suite for Networked Applications|Freescale
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------