KeyWIN32_PLUGINS_DBG_PPC 10.4, LM_BADSYSDATE出现未知错误

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KeyWIN32_PLUGINS_DBG_PPC 10.4, LM_BADSYSDATE出现未知错误

846 Views
连营张
Contributor I

hi,my version of CodeWarrior Development Studio For PA  is 10.4.0  and I use the evaluation version.However, I encountered an error as shown below:

91919_91919.pngQQ截图20151026152647.png

If you can help me answer this question, I would be very grateful.

Labels (1)
0 Kudos
Reply
1 Reply

600 Views
trytohelp
NXP Employee
NXP Employee

Hi,

You're using CW for PA v10.4.

The evaluation version includes a 30 days professional license file.

When the evaluation time expires the tool will work at Special Edition level with is free of charge but limited.

According to the license file it seems the evaluation time expired the January 1st 2015.

Since the 2nd January the tool is working at special edition level.

I don't remember what was included in Special Edition for PA V10.4 and the info is not anymore available on web (contacted the team to solve it).

For me, the error message you met is normal as the evaluation time expired.

Now the question is: did you purchased a suite ?

CW for PA V10.5 is the last version.

This version is available under CodeWarrior Development Suite for Networked Applications.

For details I recommend you to refer to the web link:

    CodeWarrior Suite for Networked Applications|Freescale

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply