Dear,
Please. Can I known which are the I2C pins on RT117H?
I only know two I2C (5 and 6):
SBCL: CON_I2C6_SCL (GPIO_LPSR_07 (R8))
SBDA: CON_I2C6_SDA (GPIO_LPSR_06 (P8))
SBCL: CON_I2C5_SCL (GPIO_LPSR_05 (N8))
SBDA: CON_I2C5_SDA (GPIO_LPSR_04 (N7))
Can I known which are the 1, 2, 3 and 4 I2C pins on RT117H?
Thanks a lot!
Rubens Júnior
RWTECH
已解决! 转到解答。
Hi @rubensjunior,
In the case of the RT117H, you can also refer to "Table 11-1. Muxing Options" from the RT1170RM to find the pin muxing options of your RT117H (In this case, LPSPI1-4).
BR,
Edwin.
Hi @rubensjunior,
In the case of the RT117H, you can also refer to "Table 11-1. Muxing Options" from the RT1170RM to find the pin muxing options of your RT117H (In this case, LPSPI1-4).
BR,
Edwin.