I2C pins on RT117H / RT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C pins on RT117H / RT1170

Jump to solution
2,514 Views
rubensjunior
Contributor IV

Dear,

Please. Can I known which are the I2C pins on RT117H?

I only know two I2C (5 and 6):

  • SBCL: CON_I2C6_SCL (GPIO_LPSR_07 (R8))

  • SBDA: CON_I2C6_SDA (GPIO_LPSR_06 (P8))

     

  • SBCL: CON_I2C5_SCL (GPIO_LPSR_05 (N8))

  • SBDA: CON_I2C5_SDA (GPIO_LPSR_04 (N7))

Can I known which are the 1, 2, 3 and 4 I2C pins on RT117H?

Thanks a lot!

Rubens Júnior

RWTECH

 

i.MX-RT1170 

Tags (1)
0 Kudos
Reply
1 Solution
2,489 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @rubensjunior,

In the case of the RT117H, you can also refer to "Table 11-1. Muxing Options" from the RT1170RM to find the pin muxing options of your RT117H (In this case, LPSPI1-4).

BR,
Edwin.

View solution in original post

1 Reply
2,490 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @rubensjunior,

In the case of the RT117H, you can also refer to "Table 11-1. Muxing Options" from the RT1170RM to find the pin muxing options of your RT117H (In this case, LPSPI1-4).

BR,
Edwin.