sbc fs6500

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sbc fs6500

跳至解决方案
298 次查看
JhonYF
Contributor II

JhonYF_0-1715577323447.png

The image above is part of the FAIL SAFE STATE MACHINE,what the "POR_FS" mean?

 

0 项奖励
1 解答
294 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

POR_FS means "Power on reset for Fail Safe state machine". It is internal logic signal of FS65 and generate inside FS65. It is the condition for state transition of Main state machine and Fail Safe state machine after power on FS65 with plugging battery.

So POR_FS cannot be triggered by Wake up. "POR_FS" is just the condition for "Wake up" to "Buck or Buck Boost configuration detection Power". If POR_FS is '1', Main state machine will go from "Wake up" to "Buck or Buck Boost configuration detection Power", otherwise it will stay on "Wake up".

BR, Tomas

在原帖中查看解决方案

0 项奖励
2 回复数
295 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

POR_FS means "Power on reset for Fail Safe state machine". It is internal logic signal of FS65 and generate inside FS65. It is the condition for state transition of Main state machine and Fail Safe state machine after power on FS65 with plugging battery.

So POR_FS cannot be triggered by Wake up. "POR_FS" is just the condition for "Wake up" to "Buck or Buck Boost configuration detection Power". If POR_FS is '1', Main state machine will go from "Wake up" to "Buck or Buck Boost configuration detection Power", otherwise it will stay on "Wake up".

BR, Tomas

0 项奖励
238 次查看
JhonYF
Contributor II
Thanks for your reply!
0 项奖励