sbc fs6500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sbc fs6500

Jump to solution
445 Views
JhonYF
Contributor II

JhonYF_0-1715577323447.png

The image above is part of the FAIL SAFE STATE MACHINE,what the "POR_FS" mean?

 

0 Kudos
Reply
1 Solution
441 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

POR_FS means "Power on reset for Fail Safe state machine". It is internal logic signal of FS65 and generate inside FS65. It is the condition for state transition of Main state machine and Fail Safe state machine after power on FS65 with plugging battery.

So POR_FS cannot be triggered by Wake up. "POR_FS" is just the condition for "Wake up" to "Buck or Buck Boost configuration detection Power". If POR_FS is '1', Main state machine will go from "Wake up" to "Buck or Buck Boost configuration detection Power", otherwise it will stay on "Wake up".

BR, Tomas

View solution in original post

0 Kudos
Reply
2 Replies
442 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

POR_FS means "Power on reset for Fail Safe state machine". It is internal logic signal of FS65 and generate inside FS65. It is the condition for state transition of Main state machine and Fail Safe state machine after power on FS65 with plugging battery.

So POR_FS cannot be triggered by Wake up. "POR_FS" is just the condition for "Wake up" to "Buck or Buck Boost configuration detection Power". If POR_FS is '1', Main state machine will go from "Wake up" to "Buck or Buck Boost configuration detection Power", otherwise it will stay on "Wake up".

BR, Tomas

0 Kudos
Reply
385 Views
JhonYF
Contributor II
Thanks for your reply!
0 Kudos
Reply