Hello, I have purchased the SDK frdm-k64f with the FRDM-FXS-MULT2-B.
I have downloaded the windows sensor fusion tool and followed the instructions: installed drivers, etc. The board is running fine but the windows tool is not the same version as the sensor fusion manual is showing. For example there's no accelerometer calibration tab and there's no gyro bias calibration mode at startup. Is there a professional version of the tool or something I'm missing here?
Thank you
Hello,
After some search, I've found the latest version of the sensor fusion toolbox for windows:
regards,
You're welcome!. I've been for a long time searching for clear and detailed information about sensor fusion and thanks to NXP website (and your dedication of course) I've learned a lot. This information and available SDK's are a must for people to exploit MEMS sensors potential!
PD: I've downloaded sensor fusion toolbox V7 and working fine on FRDM-K64F / FRDM-FXS-MULT2-B. I have an issue with the bluetooth communication that I hope to get sorted soon.
Hello Mike,
Yes, I downloaded from the link you mention, more precisely from here: NXP® Sensor Fusion|NXP
It's a 35.7 Mb .rar file (SensorFusionToolboxForWindowsSetup.rar) and the .msi file inside (the windows installer) is from 14 September 2015 (quite old I think). I will dump some screenshots later on.
thank you very much for your help and the great work on sensor fusion.
Javier.
Did you download it from http://www.nxp.com/sensorfusion ? If not, you probably have a different tool (Maybe the Sensor Toolbox, whereas you need the Sensor Fusion Toolbox). There is only one version of the Sensor Fusion Toolbox, which you should get from the link above. If that doesn't solve your problem, please attach a couple screen dumps so I can see what you have.
Regards,
Mike