PCF8883 evaluation board (OM1105)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8883 evaluation board (OM1105)

1,449 Views
stanislascottar
Contributor I

Hi, I have the PCF8883 evaluation board (OM1105) and I want to make a proximity detection around 1cm with the third plate (CP3) but I only manage to have around 2 mm detection with the max value for CCPC (CU6)...

Is it possible to have 1cm detection with the PCF8883 or should I find another way ?

Labels (2)
0 Kudos
Reply
2 Replies

1,160 Views
david_diaz
NXP Employee
NXP Employee

Hello Stanislas,

The most important side effect of increasing Ccpc is that also the noise sensitivity increases.

At this point, I would like to suggest the documents attached to this response in order to improve your design since the capsensor device has three parameters that influence the switching behavior as shown in the FAQs file.

 

I hope this material helps.

 

Best Regards,

David

0 Kudos
Reply

1,160 Views
stanislascottar
Contributor I

Hello David,

Thank you for your answer, even when I worked on the three parameter I didn't manage to get to 1cm proximity... I actually wonder if this capsensor is a good choice for my application.

Best regards,

Stanislas

0 Kudos
Reply