If the MP3V5050V is operated on a 3 Volt button cell/battery, will the output voltage for the pressure measurement change/decrease as the battery voltage decreases?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If the MP3V5050V is operated on a 3 Volt button cell/battery, will the output voltage for the pressure measurement change/decrease as the battery voltage decreases?

808 Views
pmo
Contributor I

1) If the MP3V5050V is operated on a 3 Volt button cell/battery, will the output voltage for the pressure measurement change/decrease as the battery voltage decreases?

 

2) Should I use a voltage regulator in my circuit for the supply voltage to the MP3V5050V?

I am trying to conserve the coin battery power so power efficiency is important. I know that a switching regulator in the correct configuration will most likely extract more energy from a dying battery than a linear regulator which will eventually drop out. I am not certain whether noise generated from the switching regulator affect the pressure measurement?

3) How sensitive is the MP3V5050V to switching noise?

4) Can you recommend a switching regulator or a linear regulator that might work? Thank you.

 

Best regards,

 

Phil Morello

Electronic Engineer

Suspended Animation Inc.

0 Kudos
Reply
1 Reply

694 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Phil,

Since the sensor output is ratiometric with the supply voltage, any variation in supply voltage will also proportionally appear at the output of the sensor. However, it should continue working when the battery voltage decreases, but the accuracy and linearity spects mentioned in the datasheet would change with a supply voltage below 2.7V (operating the device at a different range may induce additional error).

 

You can use the MP3V5050V without the need of a voltage regulator between the battery and the sensor, but, you need to take in mind if the ratiometric nature of the sensor would not affect your application.

 

From the noise point of view, it is preferable to use a linear regulator rather than a relatively more noisy switching power supply, but since one of your key factors is efficiency, then I would definitely recommend you to use a switching regulator, just try to adequate de-coupling to reduce noise. A 0.33 µF to 1.0 µF ceramic capacitor in parallel with a 0.01 µF ceramic capacitor should work well for this purpose.

In case you need extra filtering, then you can use a low-pass RC filter with a cutoff frequency (650 Hz is recommended). A 750 ohm resistor and a 0.33 µF capacitor have been determined to give the best results since the 750 ohm series impedance is low enough for most A/D converters.

 

We do not have any recommendation for a switching regulator or a linear regulator.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply