Offset MPX230xDT1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Offset MPX230xDT1

284 Views
MBox
Contributor I

Hello,

we are using the MPX230xDT1 to monitor the pressure along a tube system.
While applying 5 V with a high-precision calibration source we measured this on Vout:

SensorVoltage in mV
10,167
20,188
30,176
40,162
50,142
60,170
70,162
80,192
90,178
100,207


For our appliance this Offset is too big (never had this issue before). Is there any way to manipulate/control the Offset?

Best regards

0 Kudos
Reply
1 Reply

241 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello MBox,

I hope all is great with you. Thank you for using the NXP communities.

We have a document that can be helpful, I would recommend you to follow the method mentioned in the application note AN1585 which is designed for uncompensated and not amplified pressure sensors, but you can skip this part and go directly to the amplification and offset control.

AN1585: https://www.nxp.com/docs/en/application-note/AN1585.pdf

In this application note is discussed different types of compensation and calibration methods and also includes reference circuit for the offset adjustments and amplifier interface.

I also suggest the application note AN1325 as appropriate reading on choosing an amplification circuit and how to introduce a dc offset shift.

AN1325: https://www.nxp.com/docs/en/application-note/AN1325.pdf

I hope this information helps.

Regards,

David

0 Kudos
Reply