Hallo,
we used NXP pressure sensor ,,FXPS7550DI4T1,, in our projekt. How can I finde Functional safty of FXPS7550DI4T1?
We need Fit rate of sensor.
Thanks for your reply.
Kind regards
Zeinab Prümm-Rahimi | Systementwicklung
AST (Advanced Sensor Technologies) International GmbH
Bärental 26 | 75365 Calw | Germany
T: +49 (7051) 6001-456
Zeinab.Pruemm-Rahimi@ast-international.com | www.ast-international.com
Hallo Zeinab,
please see the FIT rate from a quality engineer to the FXPS7550D, to another customer.
DESCRIPTION
FIT/MTBF rates can be calculated from the reliability qualification program result. However, although zero fails are found, the limited sample sizes used in qualifications can only proof relatively high FIT rates. FIT rates can also be calculated based on customer returns versus shipment volumes which is a more accurate value (referenced in NXP as FITCR). However, for the FXPS7550D14T1 device, there is insufficient shipment at this time to provide a FIT based on customer returns. Hence, the following is the FIT rate based of reliability qualification data, HTOL and ELFR. The assumptions are listed in the respective tables. Please let me know if you have any questions.
Use case temperature is 55C and the confidence level is 60%, then the following is the HTOL FIT rate (49):
Use case temperature is 55C and the confidence level is 60%, then the following is the ELFR FIT rate (102):
With Best Regards,
Jozef
Hi Zeinab,
the documents shouldn't be shared via the community. My collogue from commercial team has created a new case for you, #00593879 and will support you via this case. Please expect to be contacted soon via email.
With Best Regards,
Jozef