MPX5100DP: strange reading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPX5100DP: strange reading

ソリューションへジャンプ
680件の閲覧回数
andikun
Contributor I

Dear NXP tech.
I just bought an mpx5100dp sensor. I tried to read the datasheet but I don't really understand. Especially in the sensitivity which shows 45mV/kPa.

I tried to do a test to read analog arduino for each of the 900 data that has been read by five(5) MPX5100DP sensor. in free air. The following is a snippet of the Arduino reading for each type of sensors,

dp1dp2dp3dp4dp5
3032342930
3032342931
2931333032
3032342929
2931342930
3032333030
29.8833831.4530433.5758529.5655330.66047

*The last row is the average
Question:
1. Why can each sensor read differently?
2. Am I justified in subtracting each sensor output by its integer average? even if I subtract it then some will not produce a zero value. Does the company have a solution for this problem?

I need these sensors to do readings in a sample in my research so I try to make the resulting data logical. But I think this difference is illogical even though the sensors are placed in the same place at a very close distance.

Thanks.

0 件の賞賛
返信
1 解決策
652件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Andhy,

I hope all is great with you. Thank you for using the NXP communities.

In this case, the sensitivity refers to the voltage output for every kPa.

Do you mean that you are reading the atmospheric pressure? What is your local atmospheric pressure?

 

In this case, I do recommend performing an auto-zero.

I believe that this is caused for the offset error. Sources of offset errors are due to device to device offset variation (trim errors), mechanical stresses (mounting stresses), shifts due to temperature and aging. Performing auto-zero calibration technique will greatly reduce these errors. This technique can easily be implemented when an integrated pressure sensor is interfaced to an A/D and a microcontroller.

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
653件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Andhy,

I hope all is great with you. Thank you for using the NXP communities.

In this case, the sensitivity refers to the voltage output for every kPa.

Do you mean that you are reading the atmospheric pressure? What is your local atmospheric pressure?

 

In this case, I do recommend performing an auto-zero.

I believe that this is caused for the offset error. Sources of offset errors are due to device to device offset variation (trim errors), mechanical stresses (mounting stresses), shifts due to temperature and aging. Performing auto-zero calibration technique will greatly reduce these errors. This technique can easily be implemented when an integrated pressure sensor is interfaced to an A/D and a microcontroller.

I hope this information helps.

Regards,

David

0 件の賞賛
返信