MPL3115A2 temperature conversion

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPL3115A2 temperature conversion

1,012 次查看
lukaszprzeniosl
Contributor II

Hello there,

I am having a problem with understanding how to convert the the MPL3115A2 temperature readings exactly (OUT_T_MSB, OUT_T_LSB). Please consider this function:

inline static float rawTemperature2Float(const uint8_t* const rt)
{
    return ((float)((int8_t)rt[0])) + (((rt[1] >> 4) & 0x0F) * 0.0625f);
}

rt[0] = OUT_T_MSB and rt[1] = OUT_T_LSB.

The question is: Does the sign bit in MSB also determinate how should the fractional part be treated, or is it always positive? In the presented function I am always adding the fractional part. But maybe if the sign is negative, I should substract it (or multiply by -1)? Should the function look like this?

inline static float rawTemperature2Float(const uint8_t* const rt)
{
    float frac = ((rt[1] >> 4) & 0x0F) * 0.0625f;

    if (rt[0] & 0x80)

    {
        frac *= -1; // variant #1

        //frac = (1.0f - frac) * -1; // variant #2

     }

    return ((float)((int8_t)rt[0])) + frac;
}

If so, which variant in the if?

This approach gives similar results (all bits threaded for twos complement conversion):

inline static float rawTemperature2Float(const uint8_t* const rt)
{   
    int32_t temp = (((int32_t)rt[0]) << 4) | (rt[1] >> 4);
    if (temp & 0x800)
        temp = (0x1000 - temp) * -1;

    return ((float)(temp)) / 16.0f;
}

I would appreciate all help.

标签 (1)
标记 (1)
2 回复数

896 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Lukasz,

I do apologize for my delayed response, but I was on a business trip last week with a limited time to react on community questions.

In my code I use the following formula:

Temperature = (float) ((short)((RawData[3] << 8) | (RawData[4] & 0xF0)) >> 4) * 0.0625;

 

You need to get -0.0625 for RawData[3] = OUT_T_MSB = FF and RawData[4] = OUT_T_LSB = F0.

I will retest it again tomorrow when I am back in the office, but if I remember well, I really got -0.0625 for 0xFFF0.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

896 次查看
lukaszprzeniosl
Contributor II

Hello Tomas, thank you for answer.

Code-wise, your method is the same as my last one, which I found working. But yours is optimized better. Thank you for help, now everything is clear.

0 项奖励
回复