MMA8452Q Sleep, I2C and ODR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8452Q Sleep, I2C and ODR

Jump to solution
1,310 Views
johnmunroe
Contributor I

Hi

I'm hoping to simply fire a signal on an interrupt pin when motion/transient is detected. Would it be a good idea to put the device to sleep mode but set the sleep mode ODR to a reasonably high rate? When the device is in sleep mode, is I2C completely switched off such that no draining occurs?

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,017 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi John,

The advantage of the sleep mode is that the part can automatically switch to a lower ODR and another mode (usually Low Power) when inactivity is detected. The lowest current consumption is achieved when (S)MODS = 0b11 (Low Power mode) and when the sample rate is set to 1.56 Hz. Once activity (e.g. motion/transient) is detected, the accelerometer automatically switches back to the original data rate of the application and provides an activity interrupt that can be used to wake up the host processor. In the sleep mode both analog and digital blocks are still enabled.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

0 Kudos
Reply
3 Replies
1,018 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi John,

The advantage of the sleep mode is that the part can automatically switch to a lower ODR and another mode (usually Low Power) when inactivity is detected. The lowest current consumption is achieved when (S)MODS = 0b11 (Low Power mode) and when the sample rate is set to 1.56 Hz. Once activity (e.g. motion/transient) is detected, the accelerometer automatically switches back to the original data rate of the application and provides an activity interrupt that can be used to wake up the host processor. In the sleep mode both analog and digital blocks are still enabled.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply
1,017 Views
johnmunroe
Contributor I

Is there a way to switch off I2C (to reduce power consumption) during ACTIVE (whether wake or sleep)?

Thanks

0 Kudos
Reply
1,017 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi John,

No, there is not.

Regards,

Tomas

0 Kudos
Reply