MMA8451 and AN4070 for FreeFall detection. Is same for new FXLS8974?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8451 and AN4070 for FreeFall detection. Is same for new FXLS8974?

1,085件の閲覧回数
arnogir
Senior Contributor II

Hello,

We are using the MMA8451 only to detect a FreeFall, with I2C communication for the configuration, then the INT2 pin to interrupt the µC.

Now then MMA8451 is not recommended for new design.

I'm looking for replace it and the NXP website propose the FXLS8974.

It seems very similar, but I can't find the equivalent for the FreeFall.

Currentlty, I apply exactly what is said into AN4070 which is very simple.

On the chapter 6.2 it is explain exactly what configuration to do (only  7 steps) and that all!.

 

Are they the equivalent function on the FCLS8974? Are they this type of application note?

Regards

0 件の賞賛
返信
4 返答(返信)

1,023件の閲覧回数
JackITB
NXP Employee
NXP Employee

Hi Arnaud,

The AppNote can be found in the "Documentation" tab of the FXLS8974CF web page.
FXLS8974CF | Low-Power 12-Bit Digital IoT Accelerometer | NXP | NXP Semiconductors

 

0 件の賞賛
返信

1,063件の閲覧回数
JackITB
NXP Employee
NXP Employee

Hi Arnaud,
You can take a look at AN12004, available on NXP external website.
AN12004, Sensors Data Change Detection (SDCD) block overview with examples for FXLS896xAF, applicati...

It will give you some guidelines for standard event detection including freefall.

Regards,   Jacques.

 

0 件の賞賛
返信

1,055件の閲覧回数
arnogir
Senior Contributor II

Hi

Many thanks.

Exactly what I need.

This AN should be linked to the nxp website on this component!

How found or orherwise ?

Regards

0 件の賞賛
返信

1,004件の閲覧回数
AlessandroCortese
Contributor I

Hi,

i would like to do the same thing as you.

I have followed the AN 12004, page 15 and 16. 

I cannot understand the relationship between height and the value of the debounce register (32h).

Can you help me?

regards,

Alessandro

0 件の賞賛
返信