Hello,
We are using the MMA8451 only to detect a FreeFall, with I2C communication for the configuration, then the INT2 pin to interrupt the µC.
Now then MMA8451 is not recommended for new design.
I'm looking for replace it and the NXP website propose the FXLS8974.
It seems very similar, but I can't find the equivalent for the FreeFall.
Currentlty, I apply exactly what is said into AN4070 which is very simple.
On the chapter 6.2 it is explain exactly what configuration to do (only 7 steps) and that all!.
Are they the equivalent function on the FCLS8974? Are they this type of application note?
Regards