Hi Nxp Partner
We try to write firware code when we get our first version senior board (installs MM9Z1_638).
We found EXTAL& XTAL is oscillation signal and We also check all the voltage pin of MM9Z1_638 (VDDA,VDDX,VDDH,VDD2D,LTO ,RESET) is within the spec's requirement.Do you have any suggestion to check why EXTAL& XTAL no signal?
Br,
Mike Liang
解決済! 解決策の投稿を見る。
hi jozef
Should we use ic programmer to write initial firmware to mm9z1_638 before mount on pcb?
"without extal signal"can we wirte firmware to mm9z1_638 now ?
Br
Mike liang
Hi Mike,
please check the OSCE bit in the CPMUOSC register. It should be set to 1 to see an external wave on the EXTAL pin.
With Best Regards,
Jozef
hi jozef
Should we use ic programmer to write initial firmware to mm9z1_638 before mount on pcb?
"without extal signal"can we wirte firmware to mm9z1_638 now ?
Br
Mike liang
hi jozef
We add 470nf on two reset pin. We can write firmware. thanks
Br,
Mike Liang