Hi,
I am writing on behalf of a group of researchers to ask for information, if anyone have it available, about the sensor MPXV 7002dp since some parameters that we required are not specified in the data sheet, any information you can provide us is well received, please find attached a table with the parameters we are asking for we filled some parameters with the information available in the datasheet, the missing parameters are highlighted. Thank you very much in advance.
Parameter | Value | Measurement unit |
Range (Rg): It is the extreme value width of a physical variable of a sensor in real time. | -2 – 2 | kPa |
Span (Sp): It is the diversified behavior of the physical variable. | 4 | KPa |
Accuracy (Ar): The difference between the acquired physical value and the actual value. | ± 2.5 | %VFSS |
Precision (Pr): Closeness in acquired data with actual data is depicted in terms of precision. |
|
|
Sensitivity (St): The variability in output generation for a physical variable in a stochastic environment.
| 1.0 | V/kPa |
Linearity (Lr): It is the fluctuation of the acquired physical value and optimal data curve. |
|
|
Hysteresis (Hr): Variation in the physical variable when input is altered between extreme points. |
|
|
Resolution (Rl): Minimal alteration in the stochastic environment acquired by the sensor. |
|
|
Reproducibility (Rd): The capability of the sensor to generate a similar output for the same input. |
|
|
Repeatability (Rb): The ability to generate redundant data when repeated input is provided consecutively. |
|
|
Response Time (Rt): It is delay is the generation of the acquired data value | 1.0 | ms |
Hello Jose,
As you may noticed on the datasheet, the information that you requested is already characterized and covered on the accuracy parameter.
I am afraid that it is all the information available from your request.
I hope this information will be useful for you.
Regards,
David