How to caculate the AINx's voltage using register value for MC33774A?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to caculate the AINx's voltage using register value for MC33774A?

跳至解决方案
439 次查看
JhonYF
Contributor II

JhonYF_0-1704007791422.png

for ratiometric measurement, the register value is 16580, Which operation the "m%" mean?

Please give me an example of calculation,

Thanks!

 

 
0 项奖励
1 解答
383 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Let me apologize for the delay in answering your question due to the Christmas and New Year holidays.

Yes, the m% is an interesting unit. In the characteristics we use the following instead.

1.png

However, I am not sure if this makes things better to understand.

In fact the radiometric measurement is relative to VAUX/VDDC (depending on configuration).

Then it is: 3.051716 x 10^-3 / 100 * VAUX or VDDC

The 10^-3 is for the m

The % gives the / 100

Hope this makes it clear.

BR, Tomas

在原帖中查看解决方案

0 项奖励
2 回复数
384 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Let me apologize for the delay in answering your question due to the Christmas and New Year holidays.

Yes, the m% is an interesting unit. In the characteristics we use the following instead.

1.png

However, I am not sure if this makes things better to understand.

In fact the radiometric measurement is relative to VAUX/VDDC (depending on configuration).

Then it is: 3.051716 x 10^-3 / 100 * VAUX or VDDC

The 10^-3 is for the m

The % gives the / 100

Hope this makes it clear.

BR, Tomas

0 项奖励
378 次查看
JhonYF
Contributor II
@TomasVaverka,Thanks for your reply!
0 项奖励