How to caculate the AINx's voltage using register value for MC33774A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to caculate the AINx's voltage using register value for MC33774A?

Jump to solution
434 Views
JhonYF
Contributor II

JhonYF_0-1704007791422.png

for ratiometric measurement, the register value is 16580, Which operation the "m%" mean?

Please give me an example of calculation,

Thanks!

 

 
0 Kudos
1 Solution
378 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Let me apologize for the delay in answering your question due to the Christmas and New Year holidays.

Yes, the m% is an interesting unit. In the characteristics we use the following instead.

1.png

However, I am not sure if this makes things better to understand.

In fact the radiometric measurement is relative to VAUX/VDDC (depending on configuration).

Then it is: 3.051716 x 10^-3 / 100 * VAUX or VDDC

The 10^-3 is for the m

The % gives the / 100

Hope this makes it clear.

BR, Tomas

View solution in original post

0 Kudos
2 Replies
379 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Let me apologize for the delay in answering your question due to the Christmas and New Year holidays.

Yes, the m% is an interesting unit. In the characteristics we use the following instead.

1.png

However, I am not sure if this makes things better to understand.

In fact the radiometric measurement is relative to VAUX/VDDC (depending on configuration).

Then it is: 3.051716 x 10^-3 / 100 * VAUX or VDDC

The 10^-3 is for the m

The % gives the / 100

Hope this makes it clear.

BR, Tomas

0 Kudos
373 Views
JhonYF
Contributor II
@TomasVaverka,Thanks for your reply!
0 Kudos