FXAS21002C: HPF and LPF=12.5Hz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXAS21002C: HPF and LPF=12.5Hz

880件の閲覧回数
riscypayne
Contributor I

Hi Is there guideline how to choose or select HPF and LPF function for given application?

I'm using ODR = 12.5Hz and application is directional.

Would HPF reduce the drift or offset readout?

R.

ラベル(1)
0 件の賞賛
返信
1 返信

563件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello Rlscy,

LPF cutoff frequency with an 12.5Hz ODR is fixed to 4Hz.

Ftabs.PNG

You can enable the HPF filter by setting the HPF_EN bit in the CTRL_REG0. The HPF filter should remove/attenuate the average value (offset) of the ouput signals.

Anthony

0 件の賞賛
返信