Use plug & trust library for a71ch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use plug & trust library for a71ch

1,526件の閲覧回数
ziml
Contributor I

I have a running application on a nrf52840 that generates a random number, generates a keypair, hashes, signs and verifies a signature over the sss API on the SE050. I now want to use the same application on the A71CH, is this possible? According to the plug and trust MW documentation those functions were all mapped from the a71ch host library to the sss api. Where is the mapping done in the library?

As far as i understood, I should be able to edit the  fsl_sss_ftr_default.h file in a way that it compiles the sss api for the a71ch. If this is correct, is there an example that shows how I am supposed to set the defines? I cant seem to figure out how, is there a documentation that describes the dependencies? 

E.g: When I choose SSS_HAVE_APPLET_A71CH (and no other applet) the define for the T1oI2C is set, which is only needed for the SE050.

Cheers,
Lea

0 件の賞賛
返信
1 返信

1,517件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @ziml ,

 

The latest SE050 MW supports A71CH as well, you may refer to "SE-PLUG-TRUST-MW/simw-top/doc/a71ch/a71ch_miscellaneous.html#demos-and-examples-supported-on-a71ch" for more details regarding the changes made for testing with A71CH.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信