Secure Unique NFC on NTAG424 DNA Tags

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure Unique NFC on NTAG424 DNA Tags

953 Views
480eduardopena
Contributor I

Good day,

I have an ongoing project with NFC Tags, for user location, where some kind of anti-cloning feature is needed.

NTAG424 DNA have the SUN (Secure Unique NFC) functionality, which can fullfill our requests.

But the problem is how to implement backend to decrypt - check message. 

I have found some documentation here, but is so low-level that does not help our development team (mainly working with .NET).

https://www.nxp.com/docs/en/application-note/AN12196.pdf

Does anyone have some working example of backend server for SUN decryption?

Any help is appreciated, Thanks

0 Kudos
Reply
1 Reply

920 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @480eduardopena ,

 

Yes, on the Authentication Service we have APIs do verify the SUN message, but such kind of information is under NDA control, do you have a valid NDA with NXP? If yes, please create a private ticket according the following link and send your NDA to me via this ticket, I may contact the expert team then.  Please kindly refer to https://community.nxp.com/t5/Using-Our-Community-Knowledge/How-to-submit-a-new-question-for-NXP-Supp... for details. Please also tell me the ticket number when it is available.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply