VR5510 FCCU Mon ASIL B Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510 FCCU Mon ASIL B Chip

Jump to solution
850 Views
Nick_Pascoe
Contributor II

Hi,

Can you confirm if the FCCU monitoring functionality is available on the VR5510 ASIL B chipset? It seems to be unclear to me from the VR5510 Safety Manual. Table 5 indicates that is is available but Table 9 indicates it is not available.

0 Kudos
1 Solution
830 Views
Daniel_Wax
NXP Employee
NXP Employee

Yes I have confirmed the Safety manual will need to be fixed

 

The Watchdog difference is noteable

 

Daniel_Wax_0-1648740283131.pngDaniel_Wax_1-1648740283223.png

 

View solution in original post

Tags (1)
5 Replies
848 Views
Daniel_Wax
NXP Employee
NXP Employee

FCCU is available for ASIL-B version

 

From section 22 in the datasheet

Daniel_Wax_0-1648521685395.png

 

 

0 Kudos
846 Views
Nick_Pascoe
Contributor II

Thanks Daniel but in the VR5510 Safety Manual User Guide on page 26 Table 9. 'Fail-safe OTP configuration' it show that the register entry to enable the FCCU monitoring is only available in ASIL D chips. Can you confirm that this is the case? If so then the table you are referring to is inaccurate?

Many thanks,

Nick

0 Kudos
840 Views
Daniel_Wax
NXP Employee
NXP Employee

The Safety manual will need to be fixed

 

For ASIL-D device, the address 24 register value is  0b’0000 1101  (Decimal 13), and for all the ASIL-B device , this value is 0b’0000 0001 (Decimal 1)

That means for both ASIL-B and ASIL-D devices , FCCU_EN_OTP are enabled.

 

Daniel_Wax_0-1648566986681.png

 

 

 

Daniel_Wax_1-1648566986712.png

 

0 Kudos
836 Views
Nick_Pascoe
Contributor II

Hi Daniel,

So to confirm your saying the VR5510 Safety Manual document is incorrect and the FCCU monitoring is in fact available on the ASILB chipset?

 

Nick_Pascoe_0-1648570173386.png

 

0 Kudos
831 Views
Daniel_Wax
NXP Employee
NXP Employee

Yes I have confirmed the Safety manual will need to be fixed

 

The Watchdog difference is noteable

 

Daniel_Wax_0-1648740283131.pngDaniel_Wax_1-1648740283223.png

 

Tags (1)