Hi,
Can you confirm if the FCCU monitoring functionality is available on the VR5510 ASIL B chipset? It seems to be unclear to me from the VR5510 Safety Manual. Table 5 indicates that is is available but Table 9 indicates it is not available.
已解决! 转到解答。
Yes I have confirmed the Safety manual will need to be fixed
The Watchdog difference is noteable
Thanks Daniel but in the VR5510 Safety Manual User Guide on page 26 Table 9. 'Fail-safe OTP configuration' it show that the register entry to enable the FCCU monitoring is only available in ASIL D chips. Can you confirm that this is the case? If so then the table you are referring to is inaccurate?
Many thanks,
Nick
Yes I have confirmed the Safety manual will need to be fixed
The Watchdog difference is noteable