S32K1xx FTM internal loopback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1xx FTM internal loopback

672 Views
AdrianR
NXP Employee
NXP Employee

The S32K1xxSM_Rev6.pdf depicts at page 72 an internal signal path from FTM out (eg. PWM) to FTM in.

Could the author explain how this is practically achieved? I could not find this path in the reference manual.

 

adrianraileanu_0-1611219951194.png

 

Labels (1)
0 Kudos
4 Replies

625 Views
naveenm
NXP Employee
NXP Employee

Hi Mattia,

This will be available in SM version 7.1. It was a mistake in SM version 7.0 which is being corrected.

Please allow couple of days before SM version 7.1 is uploaded.

Regards,

NaveenM

0 Kudos

627 Views
mattiasecchiaro
Contributor I

Hello NaveenM,

thanks for the info.

In actual revision of SM ("S32K1XXSM_Rev7.pdf"), the procedure "Single Write PWM Output with external read-back" has been removed from par. 5.7.2.2.1.1.

Why?

 

Since the internal read back is impossible, we need an alternative to check a PWM output.

 

Regards,

Mattia.

0 Kudos

629 Views
naveenm
NXP Employee
NXP Employee

Hi Adrian, Mattia

Thanks for pointing out. This is a known issue with S32K1xx Safety Manual and actions are being initiated to address it.

In fact the internal read-back path DOES NOT exists in FTM. With the next release of SM (due in couple of days), it will be corrected.

Hope it helps.

Regards,

NaveenM

0 Kudos

648 Views
mattiasecchiaro
Contributor I

Hello,

we have the same issue:

  • how is the internal signal path achieved?
  • how is the "Single Write PWM Output with internal read-back" of pag.71 practically implemented?

 

We are using the P/N FS32K148UJT0VMHR.

 

Thanks,

Mattia.

 

0 Kudos