FS6500 FMEDA rescaling in temperature + confidence level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6500 FMEDA rescaling in temperature + confidence level

594 Views
LCampagnaEldor
Contributor I

Hello,

I use your FS6500 on my project, for the metrics of your components in my safety analysis I used your FMEDA but I need your support for 2 point:

  • I need to konw the confidence level of your FMEDA
  • I need to rescaling the result of the FMEDA on my mission profile and I don't understand how it is possible in your FMEDA, can you help us? (the actual FMEDA for FS6500 is at 26°C and it is not in line with my project)

thanks

0 Kudos
5 Replies

587 Views
r40959
NXP Employee
NXP Employee

Hello,

the FS6500 FMEDA has been reviewed, and also confirmed during a confirmation review of safety analysis. The confidence is then high.

You're right, we have assumed a mission profile for the failure rate. There is no possibility to update the FMEDA customer version for a different profile. In this case you need to contact Customer support to get a new evaluation of the failure rate based on your profile followed by the FMEDA update.

It is to be noted, that even with a different failure rate the hardware architectural metrics SPFM and LFM will be the same, only the PMHF will be impacted.

thank you

Best regards

 

 

0 Kudos

581 Views
LCampagnaEldor
Contributor I

Hello,

can you share the customer support contact?

with the confidence level "High" which % do you think? (99% or 90% or other?)

thanks

 

0 Kudos

577 Views
r40959
NXP Employee
NXP Employee

yes it is:

fs65.support@nxp.com

0 Kudos

571 Views
LCampagnaEldor
Contributor I

I try to send a mail to the address indicated but I recieve this answer

 

This is an automated message from mail system at host MAILER-DAEMON@prod.hydra.sophos.com

LCampagnaEldor_0-1675406883892.png

 

Message not delivered

Your message could not be delivered to one or more recipients. The details are attached below.

For further assistance, please contact your IT Administrator.

Message details

Failure reason:

<fs65.support@nxp.com>: host nxp-com.mail.protection.outlook.com[104.47.2.36] said: 550 5.4.1 Recipient address rejected: Access denied. AS(201806281) [DB5EUR01FT006.eop-EUR01.prod.protection.outlook.com 2023-02-03T06:43:54.551Z 08DB057AFC5ABA52] (in reply to RCPT TO command)

From:

ivan.fumagalli@eldor.it

To:

fs65.support@nxp.com

Subject:

FS6500 FMEDA rescaling in temperature + confidence level

Sent:

2023-02-03T06:43:54.000Z

 

 

can you share directly the data request from us?
confidence level in percent and temperature rescaling factor for the FMEDA?

thanks

0 Kudos

568 Views
r40959
NXP Employee
NXP Employee

Hello

then, please send an email to

 <william.sanfins@nxp.com>

best regards

 

0 Kudos