Hi
I'm using s32k144 FlexNVM.
And I need to know Physical characteristic of FlexNVM more.
1. Is FlexNVM NAND flash? (I think P-Flash is NOR Flash because of XIP)
2. What if Power off happened during Erase Sector Command in FlexNVM?
(After this happening, The sector has no change?)
3. As I know, FlexNVM has ECC. Is this application is on FlexNVM flash hardware?
How does it work? Please explain to me briefly
Thanks
Best regards
Phillip
解決済! 解決策の投稿を見る。
Hi Philip.
1. It is a NOR flash.
2. Interruption of an erase or program command can lead to corruption of the flash content.
AN12130 Production Flash Programming Best Practices for S32K1xx MCUs
Chapter 5 Common problems
https://www.nxp.com/docs/en/application-note/AN12130.pdf
3. Yes, it is implemented in FlexNVM HW.
For every 64 bits of data there are 8 parity bits.
AN12522 S32K1xx ECC Error Handling
https://www.nxp.com/docs/en/application-note/AN12522.pdf
Best regards,
Daniel
Hi Daniel.
Thank you for reply.
1. Could you please let me know the NOR Flash module name?
Best regards,
Phillip
Hi,
All the embedded flash is NOR.
BR, Daniel
Hi Philip.
1. It is a NOR flash.
2. Interruption of an erase or program command can lead to corruption of the flash content.
AN12130 Production Flash Programming Best Practices for S32K1xx MCUs
Chapter 5 Common problems
https://www.nxp.com/docs/en/application-note/AN12130.pdf
3. Yes, it is implemented in FlexNVM HW.
For every 64 bits of data there are 8 parity bits.
AN12522 S32K1xx ECC Error Handling
https://www.nxp.com/docs/en/application-note/AN12522.pdf
Best regards,
Daniel