Just received the development board soon, when I powers the S32K116-EVB from USB power supply, the corresponding light does not light up, even push reset button, no light light up.
已解决! 转到解答。
D3 not light. Seems not powered. Have you try to use another USB cable or another USB port of PC?
Please measure the voltage:
VDD at J10 Pin2
P5V0 at J10 pin3
P5V0 at J107 pin2
P5V_SDA_PSW at J107 pin3
P5V_SDA
Hi liuxing_hu,
Please follow the Getting Started with S32K116 Evaluation Board. Our engineer mentioned in the video: Please make sure the J107 is connect 2-3, this makes board powered by USB port.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
D3 not light. Seems not powered. Have you try to use another USB cable or another USB port of PC?
Please measure the voltage:
VDD at J10 Pin2
P5V0 at J10 pin3
P5V0 at J107 pin2
P5V_SDA_PSW at J107 pin3
P5V_SDA
my colleague help me to find that USB cable is the reason, before that I have tried 2 USB cables, it didn't work, could you give me the link to bug USB cable? I'm afraid I bought a fake cable