s32k116 The power light does not light up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k116 The power light does not light up

Jump to solution
2,517 Views
liuxing_hu
Contributor III

Just received the development board soon, when I powers the S32K116-EVB from USB power supply, the corresponding light does not light up, even push reset button, no light light up.

0 Kudos
Reply
1 Solution
2,495 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

D3 not light. Seems not powered. Have you try to use another USB cable or another USB port of PC?

check voltage.jpg

 

Please measure the voltage:
VDD at J10 Pin2
P5V0 at J10 pin3

MCU Power Supply - Jumper Selection.png

 

P5V0 at J107 pin2
P5V_SDA_PSW at J107 pin3J107 P5V_SDA_PSW.png

 

P5V_SDA 

P5V_SDA.png

View solution in original post

7 Replies
2,514 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi liuxing_hu,

Please follow the Getting Started with S32K116 Evaluation Board. Our engineer mentioned in the video: Please make sure the J107 is connect 2-3, this makes board powered by USB port.

Getting Started with S32K116 Evaluation Board.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,502 Views
liuxing_hu
Contributor III

Can you help me confirm whether the connector is ok by attachment, my colleague help me check the connect is ok, but the light doesn't work

0 Kudos
Reply
2,496 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

D3 not light. Seems not powered. Have you try to use another USB cable or another USB port of PC?

check voltage.jpg

 

Please measure the voltage:
VDD at J10 Pin2
P5V0 at J10 pin3

MCU Power Supply - Jumper Selection.png

 

P5V0 at J107 pin2
P5V_SDA_PSW at J107 pin3J107 P5V_SDA_PSW.png

 

P5V_SDA 

P5V_SDA.png

2,441 Views
liuxing_hu
Contributor III

my colleague help me to find that USB cable is the reason, before that I have tried 2 USB cables, it didn't work, could you give me the link to bug USB cable? I'm afraid I bought a fake cable

0 Kudos
Reply
2,492 Views
liuxing_hu
Contributor III

thanks very much for your detailed information, I will try

0 Kudos
Reply
2,512 Views
liuxing_hu
Contributor III

do you means that I need to connect pin2 and pin3 of J107 ?

0 Kudos
Reply
2,507 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

yes

S32K116EVB-QSG.png