s32k

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,201 Views
harish89
Contributor II

HI

I am using MC33664 Isolated network high-speed transceiver IC and S32k microcontroller.

Would like to know whether the DATA_RX from MC33664 should be connected to MISO pin of MCU?

 

Thanks

Harish

1 Solution
1,164 Views
guoweisun
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
4 Replies
1,160 Views
harish89
Contributor II

Hi

Thanks for the feedback

Can we get the datasheet of MC33664 updated as it is showing MOSI toward the MCU side for both DATA_TX and DATA_RX

Thanks

Harish

0 Kudos
Reply
1,171 Views
guoweisun
NXP TechSupport
NXP TechSupport

Yes, you are correct!

0 Kudos
Reply
1,167 Views
harish89
Contributor II

HI 

Thanks for the feedback.

Also, if i am using any other microcontroller apart from S32K, still we need to connect DATA_RX signal from MC33664 to MISO pin only and DATA_TX to MOSI pin right?

 

Thanks

Harish

Tags (1)
0 Kudos
Reply
1,165 Views
guoweisun
NXP TechSupport
NXP TechSupport

Yes correct!

0 Kudos
Reply