mex file not opening.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mex file not opening.

627 次查看
Mohit_Manvar
Contributor III

Hello experts,

I downloaded application note workspace from forum. I'm using S32D32 v3.4 IDE.

upon opening .mex file it is giving following error.

Mohit_Manvar_0-1710234564498.png

I also tried to import example in v3.5 and installed RTD driver version 3.0.0 but it is not opening.

 

please suggest me which IDE need to be used and which support package need to install. if possible, please provide link for download directives.

Application note link: Link 

 

regards,

Mohit

0 项奖励
回复
3 回复数

612 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Mohit_Manvar 

The example code was created using S32DS 3.5 and RTD version 3.0.0  P01 Hotfix02. To open the project please make sure to have installed the S32K3 development package and the same RTD version of the most recent releases of RTD 3.0.0 like the P07.

 

B.R.

VaneB

0 项奖励
回复

600 次查看
Mohit_Manvar
Contributor III

Hello,
I'm trying to install S32K3xx development packages but giving following error.

kindly provide solution or link from where I can download directly and install externally.

Mohit_Manvar_0-1710303794002.png

 

Regards,
Mohit Manvar

0 项奖励
回复

591 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Mohit_Manvar 

Check the following posts. There is discussed this topic, it might be useful for you. 

S32K3xx development package installation problem

S32K3xx development package could not be installed

0 项奖励
回复