CMU_FC destructive reset configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMU_FC destructive reset configuration

2,320件の閲覧回数
FabioG
Contributor III

Hi There,

1) I looking for configuring CMU_FC peripheral (Chapter 54). Revision 8 of reference manual.

There no explicit reference (I don't find it ...) about setting destructive reset, but in logic network at Chapter 24, par 8 "Clock Monitoring, page 960 "Figure 115. Frequency checking (FC) instances"  seems that to enable destructive reset we have to enable asyncronous interrupts FHHAIE and FLLAIE as shown for FC4,5,3 is it true ?

2)And why for fc0 and Fc6, in order  to enable destructive reset is activated FHHIE (Syncronous Upper threshold!! ) on the LOWER threshold path , and  for the interrupt activation   is set FLLAIE (Lower Asyncronous)for the  UPPER threshold path  ? is it a mistake or a feature ? (see attached file)

2) in revision 5 of manual there was not present FC6 (CM7_CORE_CLK). what is the difference with FC3(CORE_CLK) ?

Best Regards

Fabio

0 件の賞賛
返信
3 返答(返信)

2,296件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FabioG,

1.

This is under an internal discussion at the moment.

2.

FC_6 is available on S32K388 only.

danielmartynek_0-1710242001591.png

 

Regards,

Daniel

0 件の賞賛
返信

2,291件の閲覧回数
FabioG
Contributor III

Regarding point 1: in order to checkCMU_FC  Distructive reset, what I need to configure in CMU_FC?

Best Regards,

Fabio

0 件の賞賛
返信

2,276件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FabioG,

Based on the latest update, the diagrams should be fixed in the next RM release.

Both FLL and FHH can generate either an interrupt or reset. The destructive reset is bond with the asynchronous mode, and the synchronous mode only generate the interrupt.

 

Regards,

Daniel

0 件の賞賛
返信