i need rs485 sample code. about s32k144 sdk in IDE 3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i need rs485 sample code. about s32k144 sdk in IDE 3.4

Jump to solution
632 Views
NewMCU
Contributor I

i consider to use s32k 144 mcu. 

so we bought 144 evb board and install s32k DS v3.4 & sdk.

 

but example code not contain rs 485 code, and only have uart.

 

could you provide sample code about rs 485?

Tags (2)
0 Kudos
Reply
1 Solution
618 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as far as I know, no rs485 example is available, and moreover HW flow control is not configurable at all in the SDK, but you can manually set MODIR register.
You can refer to below thread to know how LPUART can be used.
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-LPUART-to-RS485-on-the-i-MXRT1050/ta-...

BR, Petr

View solution in original post

0 Kudos
Reply
1 Reply
619 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as far as I know, no rs485 example is available, and moreover HW flow control is not configurable at all in the SDK, but you can manually set MODIR register.
You can refer to below thread to know how LPUART can be used.
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-LPUART-to-RS485-on-the-i-MXRT1050/ta-...

BR, Petr

0 Kudos
Reply