i am building a project with S32K322 and tja1043,i need a demo for flexcan,not loopback,not canfd,not MCAL
Hi
There are currently no projects based on S32K322. The CAN PHY on S32K3X4EVB-Q172 is TJA1043. Please refer to the Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------