how to configure a S32K project with EB tresos

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to configure a S32K project with EB tresos

2,903 次查看
GaoWei149173702
Contributor I

I  configured a S32K project of CAN communication.but when I run it ,it doesn't work.there is too many parameters in a EB project,I can't configured it correctly without help.is there any document or something to read about it?or is there anywhere that I can download a Demo project that runs well?

0 项奖励
回复
3 回复数

2,879 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi GaoWei,

I remember that in your last question you used non-AUTOSAR MCAL routines in S32DS with RTD.
Do you need to use EB tresos to configure CAN routines this time?
There are routines for EB tresos in the latest S32K1 Real-Time Drivers Version 1.0.1 for your reference

SW32K1_RTD_4.4_1.0.1_D2202.png

After install it, you should be able to import Can_example_S32K144 routine with tresos Studio 27.1.

Can_example_S32K144.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,848 次查看
GaoWei149173702
Contributor I

Hi dear Robin

I downloaded the RTD and installed it ,and I can open a example project,but when I double click it,I saw this

GaoWei149173702_0-1653471989890.png

Did I installed it wrongly?

 

0 项奖励
回复

2,865 次查看
GaoWei149173702
Contributor I

Hi dear Robin:

I  clicked S32K1 Real-Time Drivers Version 1.0.1 and opened the link ,and only saw this:

GaoWei149173702_0-1653361271989.png

Do I need to pay for the RTD or buy something to get it?

0 项奖励
回复