We are developing VCU with S32K, we expect to flashing based on UDSonCAN and I found a file named " Unified bootloader user guide " introduced about it . But how could i get NxpOpenBus.exe and the unified bootloader source code? I have created a ticket ,thanks a lot.
Solved! Go to Solution.
Hi William,
Unified Bootloader Framework Unified bootloader stack based on UDS and CAN/LIN TP protocol. NxpOpenBus has been sent to you through that case.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi William,
Unified Bootloader Framework Unified bootloader stack based on UDS and CAN/LIN TP protocol. NxpOpenBus has been sent to you through that case.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions.
1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important.
2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures.
I need the reply as soon as possible since I have to send a project very soon.
Thank you for all,
Jon Ander Amante Jorge
I also need the NXPOpenBus.exe, could you send me one?
Hi Robin:
I also use S32K to develop Bootloader, so i want NxpOpenBus too. Could you share me one?