how could i get NxpOpenBus and the unified bootloader source code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how could i get NxpOpenBus and the unified bootloader source code?

Jump to solution
1,463 Views
William-Lee
Contributor II

We are developing VCU with S32K, we expect to flashing based on UDSonCAN and I found a file named " Unified bootloader user guide " introduced about it . But how could i get NxpOpenBus.exe and the unified bootloader source code? I have created a ticket ,thanks a lot.

  • Case: 00455919
0 Kudos
1 Solution
1,454 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi William,

Unified Bootloader Framework Unified bootloader stack based on UDS and CAN/LIN TP protocol. NxpOpenBus has been sent to you through that case.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
1,455 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi William,

Unified Bootloader Framework Unified bootloader stack based on UDS and CAN/LIN TP protocol. NxpOpenBus has been sent to you through that case.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
133 Views
JonAnder_Amante
Contributor I

Hi, 

I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions.

1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 

2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. 

I need the reply as soon as possible since I have to send a project very soon. 

JonAnder_Amante_0-1714631712015.png

 

 

 

 

 

 

 

JonAnder_Amante_1-1714631712034.png

 

 

 

 

 

 

 

JonAnder_Amante_2-1714631712036.png

 

 

 

 

 

 

 

JonAnder_Amante_3-1714631712047.png

 

 

 

 

 

 

 

JonAnder_Amante_4-1714631712046.png

 

 

 

 

 

 

Thank you for all, 

Jon Ander Amante Jorge

0 Kudos
796 Views
WenbinZ
Contributor I

I also need the NXPOpenBus.exe, could you send me one?

0 Kudos
1,379 Views
gangx
Contributor I

Hi Robin:

I also use S32K to develop Bootloader, so i want NxpOpenBus too. Could you share me one?

0 Kudos