i am building a project with a sbc called fs2322b ,but there is no examples can be helpful ,what i can find is only below ,but it is not useful for me,
so is there some other example that can be provided to me ,thank you .
then, when i read the datasheet of fs2322,there are some verbs i can not understand ,like below:
what's meaning of otp fuse,i need your help ,as soon as possible,
已解决! 转到解答。
Hello,
I am not aware of any other FS23 software drivers and code examples.
OTP fuse means that the value of these bits depends on their OTP configuration. For example, the LIN_EN bit will be 0 (= LIN disabled) if the corresponding LIN_EN_OTP bit is 0. Similarly, the LIN_EN bit will be 1 (= LIN enabled) if the LIN_EN_OTP bit is 1.
In case of the FS2322B, LIN_EN_OTP = 0 (= LIN disabled) and consequently LIN_EN is also 0.
BR, Tomas
Hello,
I am not aware of any other FS23 software drivers and code examples.
OTP fuse means that the value of these bits depends on their OTP configuration. For example, the LIN_EN bit will be 0 (= LIN disabled) if the corresponding LIN_EN_OTP bit is 0. Similarly, the LIN_EN bit will be 1 (= LIN enabled) if the LIN_EN_OTP bit is 1.
In case of the FS2322B, LIN_EN_OTP = 0 (= LIN disabled) and consequently LIN_EN is also 0.
BR, Tomas