I have written a driver to program a S32K118 device and now I can program the program flash, but when I write to the FlexNVm address (0x1000000) as I program the program flash, I get an error while reading FTFE_FSTAT .
Can someone tell me what is the sequence to program flexNVM? (used like flsh)
已解决! 转到解答。
Hi,
Thanks your information, it's usefull.
How do I program the D-flash area once I have partitioned it?
Because the "Program Phrase" and "Program section" commands can only program 24-bit addresses, and the address of D-Flash starts from 0x10000000, which requires a 32-bit address.
Thanks
Mario
Hi
now i can program the area of flexNVM but except the first 0x800 addresses
do you know why?
I discovered that 0x800 is the size of flexRAM and I always find "0x33CC6699F0F055AA" at the first address of FlexNVM (0x10000000) can this information be useful?
Thanks
Mario
I haven't encountered a similar problem. In theory, there should be no data. Maybe the device has been partitioned before.
I suggest that you perform a mass erase on the device first, then partition the device, and then try to read and write to the FlexNVM area.
Hi
I found an interesting pattern, in fact I can program the first sector of flexNVM.
But once I disconnect and reconnect the power, the first sector of FlexNVM is automatically modified to the value "0x33CC6699F0F055AA" and "0xFF..."
it's wired.
Do you have any thoughts on this?
Thank
Mario
/*********************************************************************************/
Thanks you
I already understood why.
is my problem.
already solved
/*******************************************************************************//
If you need to use the 32kb space of flexnvm as D-Flash, you need to partition it first.
you can refer to AN11983