Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA

ソリューションへジャンプ
1,166件の閲覧回数
vijayvaidya
Contributor I

Hello,

After going through the schematic for the said EVB (S32K148EVB-SCH-29644-RB.pdf), we find that the EVB 'can be' used to Flash/Debug a S32K148 based external custom hardware, through J20 connector and managing 'Isolation Resistors'

But there is no specific mention of this facility either in Quick Start Guide (S32K148EVB-QSG.pdf) or User Manual (S32K148-UM.pdf).

Can somebody confirm this and if yes, with what modifications.

We intend to use the EVB that is available with us for this intended application for our new project based on S32K148.

Thank you very much

Regards,

- Vijay Vaidya

 

 

0 件の賞賛
返信
1 解決策
1,140件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I'm afraid it can not achieve.

You can refer this: Can't flash elf to S32K146Q100 by OpenSDA

 

Best Regards,
Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,141件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I'm afraid it can not achieve.

You can refer this: Can't flash elf to S32K146Q100 by OpenSDA

 

Best Regards,
Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,130件の閲覧回数
vijayvaidya
Contributor I

Hello,

Thanks Robin_Shen for your inputs.

Regards,

- Vijay Vaidya

 

 

0 件の賞賛
返信